GANTRY.STATE

Description

State  
GANTRY.STATE 0 Each axis is individually controlled.
GANTRY.STATE 1 Gantry is pending successful homing.
GANTRY.STATE 2 Gantry Mode is pending successful re-homing.
GANTRY.STATE 3 Gantry Mode is active, issue commands on Axis 1.

By default, a dual axis drive is configured for each axis to be individually controlled. In this mode, GANTRY.STATE = 0.

When an axis is put into Gantry Mode (AXIS#.CMDSOURCE = 4), the Gantry is configured but full gantry mode cannot occur until both axes have been homed. In this mode GANTRY.STATE = 1. Amp Enable is now controlled through Axis 1, but both axes are running their own trajectories until both axes have been successfully homed.

As soon as both axes have been successfully homed, GANTRY.STATE will be 2 indicating Gantry mode is active and now all motion is controlled through Axis 1 under a single trajectory generator.

If any axis has its home offset cleared (AXIS#.HOME.CLEAR) homing will need to be completed for both axes again.

Versions

Action Version Notes
Implemented 02-02-02-000  

General Information

Type Read Only
Description Reads Gantry status
Units N/A
Range 0-2
Default Type 0
Data Type Integer
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

GANTRY.STATE

300eh

05h

Unsigned8

-

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

GANTRY.STATE

3003

BBB

Unsigned8

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

GANTRY.STATE

3003

Unsigned8

Read Only

-